Part Number: TPD1E6B06 Hi Sir
I have two questions for you:
1) Dose TPD1E6B06 has any test report to prove it can pass "IEC 61000-4-2 Level 4 ESD Protection" test ?
2) Dose TPD1E6B06 has any report to prove it has ROHS / REACH ?
Part Number: TPD1E6B06 Hi,
ESD protection on SPI lines
We are considering using ESD protection elements for SPI lines. Is there no problem using TPD1E6B06?
best regards
Other Parts Discussed in Thread: TPD1E6B06 Hi Team,
On a usb 5v supply, which is better for esd human handling protection, double-backed diode or single-ended tvs diode?
Do you have any 0201 size recommendations? I have seen the https://www.ti.com…
Brian,
The cross would be the TPD1E6B06. Note that this is for 5V working voltages.
Also the TPD1E6B06 has a higher ESD rating and surge rating. What application is this going on?
Regards,
Cameron
Hello Saurabh.
For a P2P bidirectional single channel part with 5 V Vrwm in a 0201 package, the only suitable device I found was TPD1E6B06. Unfortunately, this part has a much higher capacitance at 6 pF.
However, if it's possible to switch to…
Hi Ann,
SN74LVC1G3157 is the best recommendation against the NC7SB3157P6X. But as you observed the SN74LVC1G3157 is 2kV. Our recommendation would be to use a discrete protection diode near the external port. This would give the best level of protection…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…