Part Number: TPD2E2U06 Hi
I am using TPD2E2U06DRLR for protect USB application and schematic as show below
and the layout example as show below
as show in the FIG 12 Pin 2 and 5 is connecting but in the table as show below
as show in the table Pin 2…
Part Number: TPD2E2U06 Other Parts Discussed in Thread: TMUX1072 , TS5A623157 , , TPD1E05U06
Team,
The use case is the below: On a PCB an I2C master communicates to an I2C slave over an analog MUX (like TMUX1072, TS5A623157). IEC61000-4-4 Burst events occur…
Part Number: TPD2E2U06-Q1 Hi TI-team
My customer has a question.
They think this part is a diode that can be used in Ethernet for vehicles.
Is the following satisfied ?
- OPEN ALLIANCE:IEEE 100BASE-T1 EMC Test Specification for ESD suppression device…
Back to Interface Home Page
I2C Protection
Highlights:
2 Lines to Protect
Low Capacitance required to minimize signal interference
Speeds up to 5Mbps
TI Products Recommendations
Working Voltage (V)
IEC 61000-4-2 ESD Rating (kV) (Contact) …
Part Number: TCAN3413 Other Parts Discussed in Thread: TPD2E2U06 , Hi team,
Is there any concern that a customer use 5.5V ESD protection device like TPD2E2U06 for CANH/CANL in industrial application?
Customer is going to use CAN FD interface between a sensor…
Part Number: TPD2E2U06 Hi,
what is its maximum clamping voltage of the TPD2E2U06?
Data sheet DC table is stating low voltage for clamping , but it's looks like 60V according to the ESD graph on the datasheet
Thanks
Moshe
Part Number: SN65240 Other Parts Discussed in Thread: TPD2E2U06 , TPD4E05U06 Hi team,
Is a new version of this product available for my customer's new designs? Thanks!
Best regards, Sam Ting
Part Number: TPD2E2U06-Q1 Hi,
I have a battery in series with a fuse followed by a TVS for reverse polarity protection.
Let us say, my fuse takes 10ms to blow at 40A when I reverse connect the battery.
How do I coordinate the TVS and fuse, such that the…
Part Number: TPD2E2U06-Q1 Hi,
Can you help tell me the test method of line capacitance CL in the datasheet?
My customer wants to know how to confirm the maximum value of this spec. (1.5pF, 1.9pF)
It will be appreciated to share the test instruments part…
Part Number: TPD2E2U06 Hi,
Good day!
Our customer wants to know the difference between TPD2E2U06DRLR-P and TPD2E2U06DRLR. Also, we wants to know if what does "-P"means.
Looking forward to your response.
Regards,
Cedrick