Part Number: TPD2EUSB30 Hi Team,
My customer is requesting for the abs max junction temp of our TPD2EUSB30DRTR. Kindly advise since this is not stated in the datasheet.
Thanks!
BR,
Alfred Logico
Part Number: TPD2EUSB30 Hello,
Could you provide a spice model for part TPD2EUSB30?
I'd like to use it with a custom driver (so not USB) due to its very low capacitance, but I need to simulate the effect it has on the voltage.
Best regards.
Part Number: TPD2EUSB30 Dear Specialists,
My customer has a question about TPD2EUSB30.
I would be grateful if you could advice.
--
5.5V or more is applied to TPD2EUSB30 and the Zener breakdown occurs, and Iz = 30mAmax continues to flow.
Will…
Part Number: TPD2EUSB30 Hi,
Just wondering if you've done any characterisation of the TPD2EUSB30 for Superspeed Plus (10Gbps) lines?
Best regards,
Jørgen
Part Number: TPD2EUSB30 I have a customer wanting to use a single ESD device for multiple applications.
Can this device be used in any of the following applications? Are there any extra design concerns...?
- USB3.0 - DP - LVDS - Ethernet
Part Number: TPD2EUSB30 Other Parts Discussed in Thread: ESDS314 , TPD4E05U06 , TPD4E1U06 , ESDS304 , TPD2E2U06 Hi team,
I am looking for a transient voltage protection for SGMII CML lines (1.25Gbps + 100ppm), rise time is 60 to 300ps. Total jitter…