516582e_vayu_evm_28aug_2013a.pdf Tsvetolin Shulev,
I have tried as you suggested.
Now the "mmc0: host does not support reading read-only switch, assuming write-enable" message is coming" after the below modification in DTS File.But still the File…
0160.sprr212.pdf 3107.CPU_Schematic.pdf Hi Rishabh,
Please find the attached schematic and layout.
In schematic U6 NAND IC present in out EVM.
Could you please confirm,whether we are referring correct schemtic and Source code?
Regards,
Sankar…
sprr212.pdf CPU_Schematic.pdf Hi Shravan,
Thanks for reply.
Please find the attached schematic and layout.
In schematic U6 NAND IC present in out EVM.
Could you please confirm,whether we are referring correct schematic and Source code?
Regards…
Fullscreen
8400.app_log.txt
Download
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
381 bytes read in 3 ms (124 KiB/s)
Running bootscript from mmc0 ...
## Executing script at 82000000
Partition Map for MMC device 0 -- Partition…
Hi Jim,
The Fs value of 1000Msps with JMODE0 was selected at the GUI; so for both channels of the ADC, the JESD protocol uses the first four lanes, which are connected to the transceiver pins of the FMC connector. The signal to be sampled was 100mVpp…
a10_soc_devkit_03_31_2016.pdf Thanks JIM
Pls confirm whether u have checked with "DK-DEV-1SGX-L-0A" or "DK-SOC-10AS066S-A" just in case i am attaching the scematic of "DK-SOC-10AS066S-A". Kindly look at the FMC site A & B whichever is suitable.
you…