Part Number: TPD2S701-Q1 Hi team,
I would like to protect an UART going from an ECU to another in an automotive environment. This means I have to protect TX/RX against Short-to-batt (12V automotive battery) and Short-to GND.
Do you see any devices in…
Part Number: TPD2S701-Q1 Hi Team,
Regarding the TPD2S701-Q1 EVM, it includes components such as T1, L1, and L2. Could you please explain the function of L1/L2 with a value of 10nH? Moreover, in real projects, would there be a need to use L1 and L2?
…
Part Number: TPD2S701-Q1 Other Parts Discussed in Thread: TPD6S300
Hi Team,
Customer would like to design TPD2S701-Q1.
Would you please help review schematic and provide your comments?
1. Please assist in providing detailed specifications for the ESD…
Part Number: TPD2S701-Q1 Hi,
Is there any power on sequence requirement for TPD2S701?
If direct tied /EN to GND, is it okay?
Thanks and Best regards,
Tiger
Part Number: TPD2S701-Q1 Other Parts Discussed in Thread: TPD2S703-Q1 Hi Team,
Is the TPD2S701-Q1 interchangeable with the TPD2S703-Q1 without any hardware change?
Thanks!
Roy
Part Number: TPD2S701-Q1 Hi team,
Do we have the Minimum Peak Pulse Power Dissipation data in Watts like below Transient Voltage Suppressor Diode? My customer treat TPD2S701-Q1 as TVS diode. They need this kind of data to approve AVL code.
Thanks.
https…
Part Number: TPD2S701-Q1 Hi,
I would like to double check whether it is okay to swap D+ and D- for TPD2S701?
Suppose it is okay. Please help to double confirm, thanks!
Thanks and Best regards,
Tiger
Part Number: TPD2S701-Q1 Hi team,
I see both OVP threshold and D± Clamping Voltage can be adjusted by Vref, but D± Clamping Voltage is always larger than OVP, where VBR approximately = 0.7 V, IRDYN approximately = 1 V as stated in datasheet.…
Part Number: TPD2S701-Q1 Dear Sir.
Good day.
May I ask why USB2.0 D+/- OVP can be adjusted. I think the signal voltage level is fixed. Are there other considerations and applications? Thanks for help~
Part Number: TPD2S701-Q1 Hi Team,
As title, I'd like to know if this device supports USB 3.1 Gen 2 10 Gbps signaling rate?
If not, do we have any other device that supports this?
Thanks!
Roy Hsu