Part Number: TPD4E1U06 Hi Team,
My customer needs to comply with IEC 61000-4-4 in a battery powered device. Since this doesn't have an absolute ground they are wondering how to best dissipate surges. Do you recommend to connect the diodes to metal foil…
Part Number: TPD4E1U06 Other Parts Discussed in Thread: TPD1E01B04 , , TPD4E02B04 , ESD122 Hi
Is this one suitable for LAN 2.5G/10G? Or have a suitable product suggestion
Thank you
Part Number: TPD4E1U06 Other Parts Discussed in Thread: ESD122 , TPD2E2U06 Hi team,
I'm looking for ESD protection for MIDI port. Is TPD4E1U06 suitable for this use-case?
You can refer https://mitxela.com/other/ca33.pdf for understanding MIDI standard…
Part Number: TPD4E1U06 Hi, In our design, we are using 1G Ethernet PHY DP83867, Can the part TPD4E1U06 provide ESD protection for 1G Ethernet transmission ?
Part Number: TPD4E1U06 Hi team,
Is there any consideration that R&D should have when dealing with a charged RJ45 or RJ11 connector? Like ESD?
Any if ESD is the major concern, is there recommended ESD protection product that I can suggest to my customer…
Part Number: TPD4E1U06 Hello Guys,
Good day.
Our customer need to fill-out the attached excel file for the device electrical specifications. This is needed for the device registration of TPD4E1U06DCKR. Need your help to fill most of the parameters…
Part Number: TPD4E1U06 Hi all Would you mind if we ask TPD4E1U06? It occurs waveform distortion in using several TPD4E1U06s. We think that it depends on input capacitance. Exceptt for input capacitance, what is effective for waveform distortion? Kind…
Part Number: TPD4E1U06 Hi Expert,
The customer is used the TPD4E1U06 to replace to competitor's solution.But there is a pull high resistor (1K then wired to VDD) on the original design.Since the project is MP,the customer want to reserving pull high…
Hi Amal,
In order to know if the VBUS power line may be able to be connected to either Pin3 or Pin6 of the TPD4E1U06 for ESD protection you would need to know the magnitude of the possible ESD transients on the VBUS power line in your application. The…