Part Number: TPS2547 Other Parts Discussed in Thread: TPD4S014 , TPD4S214 Hi Team,
Customer is wondering if they need to add a OVP(in case end user add a >5V source) at our TPS2547 output side, how to protect it ?
Clamping Diode or OVP part ?
Another…
Part Number: TPD4S014 I have got question about how to connect shield and gnd of the USB socket.
In my solution I have got two options. In first case the whole housing is made from metal and it is connected to the gnd. In second case the whole housing…
Part Number: TPD4S014
Hi,
I have several questions relating to the TPD4S014 and its EVM on behalf of an engineer.
1.The TPD4S14EVM that was received upon EVM-order match the picture on the product page at TI.com. However, the EVM layout in the user's…
Hi Lyle,
The current consumption shown above is in the case there is a voltage applied to VBUS. The TPD4S014 is designed to receive power from a USB 3.0 or lower VBUS source. The current consumption is a result of needing to power the required internal…
Hello
please tell me what will be the power input to shut down the output device
when I decrease the voltage from 5V down and the current is approx. 60mA
Other Parts Discussed in Thread: TPD4S014 Hi I have a product that uses TPD4S014 with an 10uF input capacitor. I was afraid that the capacitor might get eventually charged without a pull-down resistor but I noticed that the TPD4S014 has the voltage divider…
Other Parts Discussed in Thread: TPD4S014 Hi All,
I would liketo use TPD4S014 without MCU supervision. So I want to connect ACK output directly to EN input.
Is it gonna work? Please explain. See attached picture as the explanation.
Kind regards,
Andrei…
Other Parts Discussed in Thread: TPD4S014
I’m looking at TPD4S014 and thinking that it may work. But, I am confused by the typical application drawings in the datasheet.
Our situation is we want to have a USB host port on our product. It is host…
Other Parts Discussed in Thread: TPD4S014 We have used TPD4S014 ESD protection device in one of our application in the path of USB charging circuit. IN our proto board when i connected it to Power from USB port ( connected through cable which is not h…