Part Number: TPS2547 Other Parts Discussed in Thread: TPD4S014 , TPD4S214 Hi Team,
Customer is wondering if they need to add a OVP(in case end user add a >5V source) at our TPS2547 output side, how to protect it ?
Clamping Diode or OVP part ?
Another…
Other Parts Discussed in Thread: TPD4S214 Dear Sirs,
I am looking for using an A-type connector w/o ID pin for both host and peripheral operation modes.
I need to have the CPU aware of the VBUS direction, as follows:
1. If the external VBUS is active,…
Other Parts Discussed in Thread: TPD4S014 , TPD4S214 , BQ24296 , TPD1S514 Hi, I am looking to add additional ESD protection with an OTG power solution. I have been utilizing the TPD4S014 in earlier revisions, but now that I have OTG in the design things are…
Other Parts Discussed in Thread: TPD4S214 Hello~
Would you please let me know the RΘjc (Thermal Resistance Junction to Case) of "TPD4S214"??
I'm unable to find these values on "TPD4S214" datasheet.
Thanks... C.W. :)
Sorry for misspelled, I mean TPD4S214. Not TPS2549.
Can TPD4S214 manage power conflict at VBUS output without OTG ID pin?
And it can indicate permanently so it is (conflict detected) at any pin? Important specify for me.
Should I re-write in a new thread…
Hi Aramis.
I was actually refering to tpd4s214 or a compatible component. the tpd4s214 has a 0.4 pitch and thats too small for my application.
Are you familiar with some other parts that may be suitable as USB OTG companion device?
Gilad.
Part Number: AM3358 Other Parts Discussed in Thread: TPD4S214
Tool/software: Linux
Hi All
We have a custom board loosely based on the BBB. AM3358, TPS65217C PMIC, etc. This particular device can remain in a situation where it is expected to be powered…
Sefa, TPD3S014 is designed to limit the current source (VBUS) on the system side (the IN Pin). It sounds like you are planning on having an OTG type VBUS, where the source can be on either the VBUS_Connector or the VBUS_System. While TPD3S014 will work…