Part Number: TPD5S115 Other Parts Discussed in Thread: TPD5S116 , I am supporting a customer who is considering using the TPD5S115 (or TPD5S116) for their display/HDMI interface.
However, the customer is currently facing a challenge regarding the PCB…
Part Number: TPD5S115 Other Parts Discussed in Thread: TPD4E02B04 , Hi
I am looking for an integrated solution for the interface protection since TPD5S115 needs 2 external TPD4E02B04 for ESD protection.Do we have integrated solution on it ?
Also is…
Part Number: TPD5S115 Hi support team all.
I have received the following inquiry from a customer. I would appreciate your assistance in providing an answer.
Is the TPD5S115YFFR not recommended for use on the HDMI Sink side? The HDMI standard requires…
Part Number: TPD5S115 What are the advantages of using this device in circuit design for TPD5S115? What is the help of HDMI certification? 2. HDMI audio supports multiple types. How does the HDMI source recognize the HDMI device type and output the corresponding…
Part Number: TPD5S115
Hi Sirs,
Sorry to bother you.
We see the unwanted waveform on HDMI DDC when we perform the test of HF1-55. This unwanted waveform will cause the faliure on "Hold time START condition" and "Setup time START condition" when we…
Part Number: TPD5S115 Dear Sir,
There is a customer project using TI’s TPD5S115YFFR HDMI level translator and we have a question about it.
As input 5V to the VBAT pin, the output voltage VOUT is inside what defined in datasheet: [4.9V, 5.13V]
But…
Hi Jacky & Team,
Presently datasheet is having the 3rd Page image only. It doesn't have Recommended land Pattern information. Can you please conform where i can get correct details regarding Footprint of TPD5S115.
please refer the below query. …
Part Number: TPD5S115 Hi Sirs,
Sorry to bother you.
We are test 7-13 Vcec will be fail, the voltage around 0.7 v (SPEC< 0.6)
We combine GND/PGND together on currently design,
So we think it cause 7-13 test item fail
Can you share your experience…
Part Number: TPD5S115 Hi Sirs,
Sorry to bother you.
When we test HDMI CTS 7-11, we found if machine to load 0.02mA, the output will keep normal value 5.0288v. But if load lower than 0.01~0 mA, the output will be 6.483V. There will make 7-11 test result…