Part Number: TPD6E05U06 Tool/software: Hello,
We need to do some Hyperlynx SI simulations with this component in the signal path. Could you please provide an S-parameter model or have someone reach out to us? This will be used in one of our new Ultrasound…
Part Number: TPD6E05U06 Tool/software: Could you please provide us with the CTE values for the subject part number?
We would appreciate it if you could provide the CTE values in ppm/°C or ppm/°F, as well as the temperature range over which the values…
Part Number: TPD6E05U06 Customer feedback that the USB3.0 requirements cannot be met when using this product。 Do we have the related SI mode of high speed test? Or any other experiment results? Which could convince customers that this is not our device…
Part Number: TPD6E05U06 Hi team,
May I know how to calculate the TPD6E05U06 max value of power consumption?
Can I use the “max voltage” * “max current” in TLP measurement?
And what is the TLP Plot IO to GND means shown as below?
Thanks.
…
Part Number: TPD6E05U06 Other Parts Discussed in Thread: STRIKE
Hi there,
We have used TPD6E05U06RVZR on user USB 3.0 and user HDMI interfaces. These conn could be touched by user and will bear IEC standard EMC test during verification process, so…
Hi Hudi,
Welcome to E2E!
Internally to the device there is no difference between the D+ and D- pins. You can connect any of your signal lines to any of the ESD protected channel pins of the device.
Best regards,
Andy Robles
Part Number: TPD6E05U06 I am looking for ESD protection diode for USB. I found TPD6E05U06 which is unidirectional TVS. Does this mean that protection is only over positive voltages ? and not for negative voltages ?
From the datasheet the DC breakdown…
Part Number: TPD6E05U06 I have encounter an error message : "Error : at line 197 in file Z:/IBIS/TPD6E05U06.ibs : Repeated voltage value for typical curve" When importing the IBIS model in simulation tool (Mentor Graphics HyperLynx)