Part Number: TPD6F002 Hi there,
My customer is looking for a suitable solution with the following requirement:
24-bit data Ports and LCD clock (attenuation range: 100MHz~1G over -15dB is better.
They've actually looked at TPD6F002 but the ports are…
Hi Sebastian,
Yes, we do have devices that we typically recommended for MIPI interfaces. The devices are: TPD4E1U06 , TPD2S017 , TPDxF003 (EMI filter w/ ESD), TPD6F002 (EMI filter w/ ESD).
Please let me know what you think of these recommendations or if…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation and Temperature
Top…
Other Parts Discussed in Thread: TPD4E1U06 , TPD2S017 , TPD6F002 Hello guys,
One of my customers is looking for ESD protection device for MIPI interface.
Is there any recommended device?
Your reply would be much appreciated.
Best regards, Kazuya.
Other Parts Discussed in Thread: TPD6F002 Hi
We have an application where we are using SPI protocol to communicate with external sensors.
We need to implement ESD/EMI filters on the lines, so i want to ask is the TPD6F002 suitable for the SPI lines also…
Hi Stefan,
We have two 6-ch EMI filters you could use here: TPD6F002 and TPD6F003 . They won't be P2P, the packages will be slightly larger but they are the same channel count. Unfortunately we don't offer any other EMI filters in the tiny DSBGA…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
TPD6F002 is in DSV PACKAGE with GND on central pad, on the side are two undescribed pads. You do not know whether these pad associated with the GND or is unconected? My point is whether the component can be used to one side PCB?
Cameron-san;
Thank you for your reply. Our customer will use between FPD-LinkIII signals. This line is very fast (GHz order). If they use TPD6F002-Q1, this device inserts the FPD-LinkIII lines (serial insert). In this case, does TPD6F002-Q1 impact to FPD…