Part Number: TPD6S300 Hi team,
Customer wants to test C_SBU pin, but customer want to test this from 6V~17, 18V, is this going to cause anything below?
1. Leakage
2. Burn down
I saw the absolute test case on C_SBU pin is -0.3V~24V, just would like to…
Part Number: TPD6S300 Hi Team, Can you help us on the proper connection of the RP pull-up resistor described on section 8.3.4 of the TPD6S300 datasheet? Unfortunately we can't find explicit information about where to connect this resistor within the datasheet…
Part Number: TUSB211A Other Parts Discussed in Thread: TUSB322I , TUSB542 , TPD6S300 Tool/software: Hi,
When I connected a custom board and a third-party product with USB2.0, a negotiation error occurred.
I hope that by installing a Redriver on the USB2…
Part Number: TPD6S300 Other Parts Discussed in Thread: , STRIKE Hi there,
My customer is considering using the circuit below to control the on/off of CC line. Is there any problem?
And capacitors are used on CC lines, the datasheet of TPD6S300 suggests…
Part Number: TPD6S300 Other Parts Discussed in Thread: TPD8S300A , , , STRIKE Hi Team,
My customer would like to add OVP solution on D+ and D- for USB TypeC. I think TPD6S300 also can meet customer requirement. But it look like only can use SBU1/2 path because…
Part Number: TPD6S300 Other Parts Discussed in Thread: TUSB542 , , STRIKE Hi Team
I am using TPD6S300 in our design. We are facing issue that we are able to detect superspeed in one orientation ,while we are not able to detect superspeed in other orientation…
Part Number: TPD6S300 Other Parts Discussed in Thread: , STRIKE What's the difference between TPD6S300A and TPD6S300? Which should I promote to customer?
Part Number: TPD6S300 For a configuration using the TPS65994A + TPD6S300 in source-only mode:
We do not want voltages to be fed-back into the system when it is powered down & someone connects to the USB-C port.
We are thinking that if we ground the…