Part Number: TPD6S300 Hi team,
I have a question regarding TPD6S300, per subject
Can I left SBU & C_SBU pin floating if TType-C PD's not use for DP mode?
Andy
Part Number: TPD6S300 Dear Sir,
The following is the customer's Type C port protection circuit with D1, TPD6S300, and it will be caused fail in the surgea and FET test.
Could you help to check why cause the results?
Thanks, Ian.
Part Number: TPD6S300A
Hello Expert,
My customer has question for TPD6S300A. Datasheet showed Sink side use case at page 1. However we couldn't found sink side use case.
Is this device can use for Sink Side?
Thank,
Kazuki Kuramochi
Part Number: TPS65987D Other Parts Discussed in Thread: TPD6S300
Hello,
I am using the TPS65987D for a docking station circuit which:
- Can provide Power (20V 65W; Source-Mode) over USB-C to a Tablet or Laptop PC.
- can be powered from the Laptop in…
Part Number: TPD6S300 Hi, Team, Could you teach me the Rdson variation of TPD6S300? The customer want use TPD6S300 for TBT3, but the Rdon is high. Best Regards, Satoshi Yone
Part Number: TPD6S300 Other Parts Discussed in Thread: TPD2S300 , TPD1E05U06-Q1
We are using a FTDI FT601 controller to communicate with our USB TYPE C connector. It has the following ESD protection (taken from Data sheets…
Part Number: TPD6S300 I purchased one EVB for TPD6S300. However, the top mark from the component on the EVB is "6S30P". It do not comply with DS's description. So, is it the same thing with TPD6S300? or maybe something else?
Part Number: TPD6S300 Please let me know about overvoltage function for CC1, CC2, SBU1, and SBU2 Pin for TPD6S300.
When any one line (ex. CC1) detect overvoltage, which SW off function only CC1 line or four all line?
Best regards,
Satoshi
Part Number: TPD6S300 On page 6 of the documnet "Circuit protection for your next USB Type-C™ design White Paper " says ,when CC Short-to-VBUS through a cable,during the ringing the maxium voltage can be up to 44V ?How do you get 44V? …