Part Number: TPD7S019
if the DDC channel of TPD7S019 is not used, as shown below,
1. Does Pin 7 VCC_DDC need to be connected to 3.3V?
2. Do any processing need to be done on Pin 9, Pin10, Pin11, and Pin12?
Part Number: TPD7S019 Hi,
Customer is evaluating TPD7S019 and they hope to know some spec about it.
May we know what is the value about these items as below?
Thank you.
ESD Diode Forward Current (mA)
Level Shifting N-MOSFET…
Part Number: TPD7S019 Dear Expert
Could u suggest a VGA driver, to support 1920*1080 resolution, and support display landscape and portrait rotation, help to see if there is a brand recommended ha? thank you!
Part Number: TPD7S019 Hi Team
We use TPD7S019 on VGA port. When system in S5 , The P3V3_AUX is 3.3V and P5V= 0V.
We find P5V have 1V leakage voltage. I have remove DDC pull high resistance.The leakage voltage will be fixed(R76/R77).
Is it normal…
Part Number: TPD7S019 Hi Expert,
The datasheet shows that the BYP needs to connect a 0.2uF to increases the ESD. When we add the large Cap at BYP, seems the BYP will be damage by ESD. Can you guide me it? Thanks!
Part Number: TPD7S019 hey,
According to comx carrier board specification that i am using , the termination resistor on video lines(RGB) is 150R. But in TPD7S019 datasheet i found that, the termination resistance must be 50R to75R.Please find page no…
Part Number: TPD7S019 Hello Sirs,
May I double check if our CPU Hsync,Vsync,DDC is 3.3V logic or lower .
Can I apply all power supply (Vcc_ddc/Vcc_sync/Vcc_video) to 5V ?
Datasheet application schematic apply 3.3V for Vcc_ddc .
Will sync_in1 &…
Part Number: TPD7S019 Hello Team,
Customer is using this part for a long time, but they got one design from other vendor about TPD7S019, and we have several questions about BYP pin, could you kindly help us double confirm them?
1. we recommended…
Part Number: TPD7S019 Hi,
Customer raised the question as below.
In the TPD7S019 datasheet, there is a bypass capacitor 0.22uF is showed in function diagram. We do ESD test with 0.1uF bypass capacitor, the test result is pass. Is there any concern…