Part Number: TPIC6C596 Other Parts Discussed in Thread: TPIC6B595
Hi,
I wanted to confirm the current capability of TPIC6C596. It's mentioned in the sheet the peak drain current-single output is 250mA with a pulse duration of 100us and 2% duty cycle…
Part Number: TPIC6C596 Dear TI,
I have two TPIC6C596 that are connected as follow:
The two drivers drive 16 IR Leds that are marked from 1 to 16.
I randomly chose LED number 9 for testing and I found that the current through the LED 9 slightly high…
Part Number: TPIC6C596 Hi team,
What's the difference between TPIC6C596DRQ1 and TPIC6C596DR? It seems that both are automotive 8-bit shift register.
Thanks and best regards!
Other Parts Discussed in Thread: TPIC6C596 , TPIC6B596 , TLC6C598-Q1 , TLC6C598 I would like to confirm the cascade connection for TPIC6C596 and TPIC6B596.
I think it is no problem.
Is this correct?
Best regards,
Atsushi Yamauchi
Other Parts Discussed in Thread: TPIC6C596 , TLC6C598 Hi
Please let me know the action of TPIC6C in the following conditions.
Usually, LED is driven with 5V power supply TPIC6C596.
Power supply voltage descends to 2.7V for 10 ms. In the meantime…
Other Parts Discussed in Thread: TPIC6C596 I would like to confirm the cascade operation of TPIC6C596.
How many the cascade connection of TPIC6C596 can we use? The demand is 7 or 8 cascade connections if we can.
Best regards, Atsushi Yamauchi
Hi Chris,
From our product line of view, we don't have a device that has the SPI interface with such high power, But I have one recommendation to you-TPS54201.
For relay driver, maybe you can check with our TPIC6C596 or something else, but I believe…