Part Number: TPIC8101EVM Tool/software: Do I need to update the firmware on the TIger board to use the TPIC8101EVM? The SPI responses are not functioning and I don't see a clock or int/hold output on the test points.
Part Number: TPIC8101EVM The board does not generate any INT/HOLD signal even when i program the GUI according to the instructions.
Itooks like a firmware problem like other users had with this device.
Best regards
Part Number: TPIC8101EVM
Hello there
I have an issue with my Ti-Ger board, the INT/CLK is not generated. I saw that this issue was solved in a previous thread in the forum, re-flashing the Ti-Ger board so I'm wondering if I can get the firmware and…
Part Number: TPIC8101EVM Hello,
when I connected my TPIC8101EVM card to the computer it automatically installed a driver. But when I try to start the GUI application, I get an error like "wrong driver installed or driver not installed". I would be very…
Part Number: TPIC8101EVM Other Parts Discussed in Thread: PGA450Q1EVM , PGA460 Have been using the PGA450Q1EVM kit successfully until now.
GUI is now unable to connect to USB hardware and TI-GER board led is off when plugged in.
Programming jumper is removed…
Part Number: TPIC8101EVM Hi I am suffering same problem with below situation
https://e2e.ti.com/search?q=TPIC8101EVM&category=forum
In short, INT & CLK signals are not coming out.
Thanks
Part Number: TPIC8101EVM Hi - I've seen a few posts on this and I seem to have the same issue (which is probably why our apprentice gave up trying to use this board a couple of years ago) !
I've scoped out the TCLK and INTH pins and got no signal…