Part Number: TPIC84000-Q1 Hi,
I want to develop a 125KHz transmitter with TPIC84000-Q1. The main goal of such transmitter is to transmit CONTINUOUS data information.
As long as I have been reading from the datasheet, there are two buffers of 56…
Part Number: TPIC84000-Q1 Hi,
I am developing a custom board with TPIC84134-Q1. Indeed, I am currently following the typical application circuit schematic in figure 8 pg.17 of the datasheet.
Concerning to the real impedance value of each output, there…
Part Number: TPIC84000-Q1 Hi,
Please recommend replace Allegro's A3941 suitable part ASAP. TPIC84000-Q1 is only support +105 high temperature. The customer need support +125 high temperature. Thanks!
Part Number: TPIC84000-Q1 Hi,
We want to develop an electronic device using the TPIC84000-Q1 as LF 125 KHz emitter.
We already have design and build a PCB with this parts:
USB/SPI Converter --> SPI --> TPIC84000
Different output and match circuits…
Part Number: TPIC84000-Q1 Hi,
I am trying to wake up and configure the TPIC84134-Q1 via SPI commands. Therefore, I have several issues that need to be solved:
1 - Is there any master device or SPI conversor recommended for sendind the 64 bits command…
Part Number: TPIC84000-Q1 Other Parts Discussed in Thread: TRPWS21GTEA Questions to TI support:
- can TPIC84134-Q1 reader be used with both DST80 & AES based transponders: e.g. TMS37145 and TRPWS21GTEA?
- if yes: application of TPIC84134-Q1 with both…
Kyogo,
Thanks for your post. The TPIC84125-Q1 and TPIC84000-Q1 belong to a different business unit, and I'm not sure which E2E forum they use. I will reach out to them to see how to get the answers you are looking for and update this thread when I get…
Dear Team,
Hope you are doing good. I need help from all of you since I am new in this application.
I have some technical queries regarding the TI IC TPIC84000.
Q1: There are total 8 half bridge output, which will let me connect 4 LF antenna…