Hello Edwin,
Please refer to the following application note, and let me know if you need more information: Inline Programming for TPLDs that have Inline Programming Capability
Best,
Malcolm
Hello Bogdan,
Please see below the pin assignment. The EVM datasheet should be the final one.
However, I don't understand your requirement. What is your intended programming method?
TI TPLD programmer + TI TPLD801 EVM ? Or
Different programmer…
Hi,
TPLD is sensitive to the levels of the input pins during programming because some pins are influencing the device mode. It is usually best to program the device before mounting it or ensure that the programming pins are not being driven by another…
Part Number: TPLD2001 Hi team,
My customer is currently considering adopting the TPLD2001. I understand that the TPLD family supports pre-programmed samples. Are there any quantity limitations for sample programming?
The customer is interested in…
Hi Arayman,
The reason your address is 0x61 instead of 0x01 is likely because your address pins (IO2-IO5) are floating. If you want the address to be 0x01, tie them all to ground. Also make sure you're
Make sure you temporarily configure the device…
Hi Takanobu-san,
We have TPLD, which the counter is programable, I have a 4bit counter SN74LVC393A which you could tie and AND gate to the Qa and Qb output to count to a binary 3, and we have some 4 bit shift registers that may solve your issue. Can…
Part Number: TPLD1201 Hello,
Do the pre-programmed TPLDs (with custom OPNs) have individual device markings on the housing to distinguish between the different configurations?
Thanks.
Hi Vinesh,
I'm glad it's working now!
TPLD2001 and TPLD1202 can both be programmed via I2C. The details can be found in the datasheet and in the Application Note Programming in Production with TPLD .
Regards,
Nikki
Part Number: TPLD2001 Other Parts Discussed in Thread: TPLD1201 I have completed my design with TPLD1201 and verified it using the evaluation board and TPLD programmer. I want to program a specific design directly with a microcontroller without using…
Part Number: TPLD2001 Our design requires that we reconfigure TPLD2001 between consequites operations.
SCEU034.pdf document mentions that in chapter 3.2.4 Temporarily Configuring a TPLD Device. We need to write a program for our ARM MCU that would do…