Part Number: TPLD1201 Hi team,
Our customer is currently evaluating the TPLD1201 using the TPLD1201EVM.
At present, they are performing evaluations by connecting the EVM to their target hardware and programming the device registers. However, they…
Part Number: TPLD1201 Other Parts Discussed in Thread: TPLD1202 , TPLD2001 Hi!
Using the TPLD1201, how do I design a state machine with 1 start bit, 6 bits. and 1 stopbit? When the correct 6 bits are continuously received the output shall be held high…
Part Number: TPLD1201 Other Parts Discussed in Thread: TPLD801 , , TPS65987D , TPLD-PROGRAM Hello team,
I have a few technical questions regarding the TPLD1201, TPLD801, and TPS65987D.
TPLD1201 / TPLD801 Edge Detection:
Can these parts detect…
Part Number: TPLD1201-RWS-EVM-DOC-CERT Other Parts Discussed in Thread: TPLD1201 Hello,
I’m working on a PWM generator design using the TPLD1201, and I’m seeing some unexpected behavior in simulation. I’d like to confirm whether this is expected device…
Part Number: TPLD1201 Tool/software: Hi Team,
1. The attached file is the configuration file. Please help to check any problems or not and provide advice for it!
Fullscreen
TPLD1201_250822.syscfg.txt
Download
/**
* These arguments…
Part Number: TPLD1201-RWS-EVM-DOC-CERT Other Parts Discussed in Thread: TPLD1201-DGS-EVM Condition:
Under Voltage turn-on = Vin< 9 V == Enable output high
Under Voltage turn-off = Vin >6.4 V == Enable output Low
Over Voltage turn-off = Vin<19…
Part Number: TPLD1201 Tool/software: Hi team,
My customer is considering adopting the TPLD1201. In their design, 3.3V is always applied to the VCC pin.
To minimize standby current as much as possible, what is the recommended configuration for unused…
Part Number: TPLD1201 Hi staff,
When I click "DRC" in ICS window, ICS warned "Input RST is ..."
Then, I added and tied GND. ICS reports error:
How should I do for this issue?
Burned TPLD1201 with similar design is working well. Can I ignore…
Part Number: TPLD1201 Hello,
Do the pre-programmed TPLDs (with custom OPNs) have individual device markings on the housing to distinguish between the different configurations?
Thanks.
Part Number: TPLD1201 Tool/software: I am planning to use the TPLD1201. I want to design a UART. How many inputs do I need for the circuit? Do I need a clock input? Can I use it for UART