Part Number: TPLD1201-DGS-EVM Other Parts Discussed in Thread: TPLD1201 Tool/software: I'm designing the TPLD1201 using Interconnect Studio. In order to solder it to a separate board for use, I wrote it permanently with the power supply selection to the…
Part Number: TPLD1201-DGS-EVM Other Parts Discussed in Thread: TPLD1201 , TPLD1202 Tool/software: Hello TI team,
I am currently trying to supply externally the TPLD1201 through the EVM board with 5V, as this represents the required logic voltage for…
Part Number: TPLD1201 Other Parts Discussed in Thread: TPLD-PROGRAM , Tool/software: Hi team,
Is it possible to write data to the TPLD1201 without using the TPLD-PROGRAM or EVM?
For example, is it possible to program the TPLD1201, which is already…
Part Number: TPLD1201-DGS-EVM Tool/software: Hi,
EVM demo is well works, but the IO5 doesn't output H at the following circuit:
Both IO6 and IO7 are good. I can't understand why only IO5 can't go H. Seems Z.
Using demo circuit, IO5 can out H/L…
Part Number: TPLD1201-DGS-EVM Tool/software: Hi,
I think that IO9 output H pulse during startup EVM. Is it true?
Both DFFs has L intial state, so will start L outputs for IO6 and IO7.
But after clicking [CONFIGURE] at the InterConnect Studio,…
Hi Juin,
To support these devices we use a 2 board evaluation method. 1 is a programmer ( TPLD-PROGRAM ) which can be used for any TPLD device, and the second is a device and package specific EVM (IE TPLD1201-RWB-EVM ) This system powers the device…
Hi Malcon,
The SPI header was a good suggestion. But simply switching to the SPI position didn't solve the problem.
To get to the bottom of the matter, I systematically installed and tested all subsequent versions up to ICS V1.7.3, starting with ICS…
Part Number: INTERCONNECT-STUDIO Other Parts Discussed in Thread: TPLD1201 Hi team,
My customer is currently evaluating the TPLD1201. During the evaluation, they found that the simulation results for the TPLD1201 EVM Demo were not displayed when using…