Hi Owen,
Thank you for your support.
We have summarized the results of TPLD-PROGRAM writing status in our environment based on the versions of TPLD-EVM and ICS as follows:
TPLD1201-EVM + ICS 1.5.0: Writing successful
TPLD1201-EVM + ICS 1.6.0…
Hi Frantisek,
The TPLD801 and TPLD1201 cannot be programmed without the TI programmer and EVM. TI can provide pre-programmed devices or samples.
However, TPLD1202 and TPLD2001 can be fully programmed without the TI programmer. The details can be found…
Part Number: TPLD801 Other Parts Discussed in Thread: TPLD1201 , TPLD-PROGRAM , TPLD1201-DGS-EVM Tool/software:
hi sir
if TPLD801 can do the function as the table?
thanks
Other Parts Discussed in Thread: TPLD1201 FAQ: TPLD > Current FAQ
TPLD is programmed through our software tool, InterConnect Studio (ICS) , in combination with a TPLD programmer and EVM. TPLD programmers and EVMs can be found on the “Hardware development…
Part Number: TPLD801 Other Parts Discussed in Thread: , TPLD1201 Please let me know which pins are used by the programmin interface to program the TPLD801 chip.
Beside GPI, there should be another 3 or 4 pins used as SPI interface. These are not documented…
Part Number: TPLD1201 Other Parts Discussed in Thread: , TPLD-PROGRAM Tool/software: Hi expert,
1. Can TPLD1201 Series support custom part numbers after production?
2. Can this provide that supports burning custom configurations? Or do they need to…
Part Number: TPLD1201 Other Parts Discussed in Thread: TPLD1202 Tool/software: Hello Team,
with the TPLD1201 EVM, it is possible to load the bitstream into the PLD and test it without flashing the OTP. Is it also possible to program the TPLD1202 serially…
Hi Jimmy,
1. Yes there are built in oscillators
2. The IOs change with the power supply (single power input).
3. Yes, TPLD1201 should be able to do this.
4. Please download interconnect studio to start designing with TPLD: TPLD-ICS IDE, configuration…
Hi Christian,
Is there anything specific you're looking for? We recommend looking at the TPLD1201 EVM user's guide and the ICS user's guide to get started. If you have a programmer and EVM already, you could also program the TPLD1201 Demo from ICS.…
Part Number: TPLD1201 Tool/software: Hi team,
Once the OTP memory of the TPLD1201 is programmed using InterConnectStudio, it becomes a permanent program and cannot be rewritten. Is this understanding correct?
During the design phase, you are configuring…