Fullscreen
1401.uEnv.txt
Download
# This uEnv.txt file can contain additional environment settings that you
# want to set in U-Boot at boot time. This can be simple variables such
# as the serverip or custom variables. The format of this file…
Part Number: AM62A7 Hi Team,
We are currently working on bringing up the 0x03f10 sensor on the AM62A Edge AI build.
The driver and DTBO have been successfully integrated, and we are able to capture and dump raw Bayer frames without any issues. The…
Hi Delaney,
Thanks for checking and for the detailed explanation!
I verified the scope settings and confirmed that it's not a trigger freezing issue. Even when using the F2800157 EVM board with external 2.2k ohm pull-up resistors, both SCL and SDA…
Hello Job,
Try adding the file https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/Makefile_5F00_ipc_5F00_linux_5F00_examples to the makerules folder in the top-level Linux SDK:
ti-processor-sdk-linux-am57xx-evm-09_03_06_05…
Andreas Dannenberg said: Let me experiment with this to see if I can create a working example that shows same but using a custom machine.
So I added a custom machine, as shown below, and re-built the `tisdk-core-bundle` target, and the U-Boot and Kernel…
Part Number: AM623 Tool/software:
There are two ti-dm file, one is signed, only the unsigned one is used in binman.dtsi, when use the signed one?
tony@ubuntu22:~/ti-processor-sdk-linux-am62xx-evm-11.01.05.03/board-support/prebuilt-images/am62xx-evm…
HI,
Merged k3-am62p5-sk-microtips-mf103hie-lcd2.dtso into k3-am62p5-sk.dts.
The same issue exists.
find the details below.
Logs in normal mode:
without DSS app :
root@am62pxx-evm:/dev/dri# ls -l /dev/dri/*
crw-rw----+ 1 root video 226, 0…
Hi Daolin,
Below is the log from the command specified.
root@am64xx-evm:~#
root@am64xx-evm:~# ls /usr/lib/firmware/ti-pruss | grep am64x*
am64x-sr2-pru0-prueth-fw.elf
am64x-sr2-pru0-pruhsr-fw.elf
am64x-sr2-pru0-prusw-fw.elf
am64x-sr2-pru1-prueth…
Hi Jared McArthur ,
I also wanted to share some additional observations:
When I try to record or play a wav file for 10 secs, it actually takes much more time - about 17 secs.
root@j722s-evm:~# date; arecord -d 10 -f S16_LE -t wav -c 2 -r 48000…
Part Number: AM620-Q1 Tool/software: Hi, Expert
I try to replace "ti_k3_m4_remoteproc.ko", and found some problems.
Error as below.
ti_k3_m4_remoteproc: version magic '6.6.58-ga7758da17c28-dirty SMP preempt mod_unload aarch64' should be '6.6.58…