Part Number: TPLD2001-DGS-EVM Tool/software: I obtained a TPLD2001EVM and created and configured the circuit on the editor. It is a simple circuit that just turns on the output port connected to the LED. I do not know how to make the circuit work on the…
Edit: the part number is TPLD2001-DGS-EVM instead, apologies. Another issue I see is when I fully disconnect the EVM from the programmer (P1 is unplugged) and click configure it still says programmed successfully which i know is obviously wrong as nothing…
Part Number: TPLD1201-DGS-EVM Other Parts Discussed in Thread: TPLD1201 , TPLD1202-DYY-EVM , TPLD1202 Tool/software: Hi Team,
We got error message "Device ID is not defined " when first time config TPLD1201 EVM. We didn't change and just follow the…
Part Number: TPLD1201-RWS-EVM-DOC-CERT Other Parts Discussed in Thread: TPLD1201-DGS-EVM Condition:
Under Voltage turn-on = Vin< 9 V == Enable output high
Under Voltage turn-off = Vin >6.4 V == Enable output Low
Over Voltage turn-off = Vin<19…
Part Number: TPLD2001-RJY-EVM Hi team,
I'm promoting the TPLD to my customer and I want to show them a simple function of TPLD: Feed the watchdog.
They need to feed the watchdog every 28ms and the high level pulse should be longer than 30us.
I set…
Part Number: TPLD1201-DGS-EVM Hello,
1. Is there a way to reset the TPLD? Such a kind of reset? We would like to reset the one with the MCU if necessary. 2. With the EvalBoard TPLD1201-DGS-EVM-A, I do not reach a voltage above 0.55 V at inputs I01 and…
Part Number: TPLD2001-RJY-EVM Other Parts Discussed in Thread: TPLD2001 Hi Sir,
May I request the TPLD2001-RJY-EVM PCBA file or layout file?
My client requires the file for debugging purposes.
Part Number: TPLD1201-DGS-EVM Other Parts Discussed in Thread: TPLD1201 , TPLD1202 Tool/software: Hello TI team,
I am currently trying to supply externally the TPLD1201 through the EVM board with 5V, as this represents the required logic voltage for…
Part Number: INTERCONNECT-STUDIO Other Parts Discussed in Thread: TPLD2001 , TPLD1202 , USB2ANY We have reactivated our TI PLD project from 2025.
Unfortunately, with the new version InterConnect Studio V1.7.3, we can no longer get our hardware setup…