Part Number: TPS1686 Hi,
We are now use TPS168616860NLMR and we have below issue for the design:
Can PGOOD pin floating or not?
Can /FLT pin floating or not?
Can SWEN pin floating or not?
Part Number: TPS1686 Hello,
According to the PDS, pin 1 of the TPS1686 is ILIM but the description in the pin table is for a current monitor pin. Pin 2 is labeled IMON but the description is for a current limit pin.
So... Is Pin 1 ILIM or IMON? I…
Part Number: TPS1686 Other Parts Discussed in Thread: TPS1685 Hi,
i was selected the part
TPS1686
for the purpose of load switch in my aaplication.
load rated is 29V max voltage and power is 150W.
as the selected part is unavailible in digikey…
Part Number: TPS1686 I have ordred TPS16861NLMR from TI.com for a design
I received parts marked TPS16861 so far so good
The part has auto retry fault behavior
Acording to the datasheet on page 3 it should be a latch-off
On page 22 at the bottom…
Part Number: TPS1686 Hi TIer
My customer use TPS16860NLMR in new medical ultrasound project.
Could you help me check the working frequency for charge pump we used to drive MOS in this chip?
Customer affraid the switch frequence noise will impact…
Part Number: TPS1686 Team,
We can calculate the Tss slew rate based on equation (10). What would the expected SR value be if the dVdT pin were open? Thanks!
Regards, Sam Ting
Part Number: TPS1686 Hello
Design TPS16860NLMR for 14S battery 60V system on output path
But facing startup with load about over 0.05A and then no output voltage
Please help on checking this issue
Thanks
TPS16860 SCH.pdf TPS16860NLMR test.p…
Part Number: TPS1686 Other Parts Discussed in Thread: LM5069 , TPS1663 Hi Team,
Could you give some suggestion for eFuse selection? This device will be used in a medical application, so they strictly require a highly reliable, mass-production (RTM)…
Part Number: TPS1686
Hi,
I have a question regarding the unused pin connection for TPS16861NLMR.
1. TEMP pin
If we do not use the TEMP pin function, can this pin be left open?
Or is it recommended to connect a capacitor from TEMP to GND…
Part Number: TPS1686
Hi,
We are currently evaluating the TPS16861NLMR for our system. According to the TPS1686x datasheet and the TI product page, the TPS16861NLMR is a 9 V to 80 V, 16 mOhm, 10 A integrated hot-swap/eFuse device with a 92 V absolute…