Part Number: TPS2041B-Q1 Hi Team,
What's the difference between TPS2041BQDBVRQ1and TPS2041BDBVR?
All spec the same except temperature range and AEC-Q100 qualification. Thanks.
BR,
Molly Huang
Part Number: TPS2041B Other Parts Discussed in Thread: TPS2044 , TPS2044B , TPS2043 , TPS2042 , TPS2041 , TPS2046 , TPS2045 , TPS2052 , TPS2051 , TPS2054 , TPS2057 , TPS2055 Hi team,
TPS2041B is a single port 0.5A USB current limit switch with typical…
Part Number: TPS2041B Dear Team,
Can you please advise regarding the following customer question
I need 2 devices like this, with connected outputs (please see the picture below)
Two voltages sources are always on. I am going to switch TPS2041B…
Hi,
I apologize that no one has followed up with your question. I'm going to close this thread, but if you still have a question please feel free to post a brand new thread instead of replying to this one. We will do our very best to respond within…
Hello Adam,
If you could post a scope shot of the current wave form you are seeing that you help immensely.
Looking through the TPS2041B datasheet the over current threshold is potentially as high as 1.9A which would introduce some initial delay…
Other Parts Discussed in Thread: TPS2041B Hello, all
Now we have one inquiry regarding inrush current protection on TPS2041B from our customer.
Please refer to the item below, and feedback us with your comment.
When referring Figure 10 on datasheet…
Other Parts Discussed in Thread: TPS2041B , TPS2041C Hi,
For 0.5A USB current limit protection, TPS2041C and TPS2041B seems the same in many aspects. Could someone point out their difference?
For example,
Martin Pakota pointed that TPS2041B lacks…
Other Parts Discussed in Thread: TPS2041B Hi~
Our customer will TPS2041BDBV device.
Resistance value between Out pin and GND pin is 8ohm.
In case Enable(Low) of TPS2041B, How about resistance value between In pin and GND pin? Is this 8ohm?
If…