Part Number: TUSB2046I Other Parts Discussed in Thread: TPS2044 , TUSB2046B Hi Team,
We would like to ask your help regarding the customer's inquiry below.
I am thinking about using TUSB2046 and TPS2044 to enable and disable hub downstream ports.…
Part Number: TUSB2036 Other Parts Discussed in Thread: PCM2906C , , PCM2903C , PCM2902C , TPS2044 Hi,
A custom board is configured using TUSB2036 and PCM2906C. When connecting to the USB port of the PC, the message "The power of the USB HUB is insufficient…
Part Number: TUSB2036 Other Parts Discussed in Thread: TPS2042 , TPS2044 , When I connect my USB Hub to usb port on a mac, I receive notification "USB Devise disabled" like this
The schematic is show here.
How should I fix this Schematic?
…
Part Number: TPS2044A Other Parts Discussed in Thread: TPS2044 , TPS2046B , TPS2044B TUSB2046_TPS2044A_OCS ISSUE_schematic.pdf TUSB2046_TPS2044A _abnormal operation figure.pptx
Hello!
Our circuit abnormally operate in current limit.
pls refer to…
Part Number: TUSB2046B Other Parts Discussed in Thread: TPS2044 , The hub is recognized by windows computer, and I am able to connect sacn disk usb drives, a logitech mouse, and an amazon basic keyboard, but when I connect other devices like a kingston…
This is external power reduced to 5V.
This is LDO regulator connected from +5V USB upstream power
I connected +5V_BUSIN0 from USB_upstream power and +5V_BUS from 5V regulator together and provided to Power distribution switch (TPS2044).
There…
I get a Unknown usb device ( Decide Descriptor Request Failed ) on Windows 10 device manager. There are two downstream devices connected and 5 open USB ports, but they never get power since the PWR on signals to the TPS2044 parts never go active ( low…
Part Number: TUSB2046B Other Parts Discussed in Thread: TPS2044 I have designed a individual-power non-ganged mode usb hub.
so upstream usb D+/D- and gnd been connected to the board/ic, but not the usb_5V, we using external input power.
this is the…
Part Number: TPS2041B Other Parts Discussed in Thread: TPS2044 , TPS2044B , TPS2043 , TPS2042 , TPS2041 , TPS2046 , TPS2045 , TPS2052 , TPS2051 , TPS2054 , TPS2057 , TPS2055 Hi team,
TPS2041B is a single port 0.5A USB current limit switch with typical…
Part Number: CD54HCT4051 Other Parts Discussed in Thread: TPS2552 , TPS2044 , TPS2054 I need some technical advice. We are doing a test card for our internal testing. We have few requirements
We need to fan out same voltage with output of x8 ,one…