Part Number: TPS2051C Other Parts Discussed in Thread: TUSB320 Dear Specialists,
My customer is considering TPS2051C and has a question.
I would be grateful if you could advise.
---
(1) When using TPS2051C on the device side, is the output capacitance…
Part Number: TPS2051C Hello,
Regarding to FLT pin on TPS2051C, my customer is asking a question.
(Question)
In their application, before 5V is input to IN pin, 1.8V is input to FLT pin while about 80ms.
1.8V (FLT) (80ms) -> 5V(IN)
At that…
Part Number: TPS2051C We didn't see the TPS2051C part is on the UL's llist as below link. Please help on this. thanks.
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/showpage.html?name=QVGS2.E169910&ccnshorttitle=Protectors,+Low-voltage+Solid…
Part Number: TPS2051C Other Parts Discussed in Thread: TPS2051 , , TPS2051B Hello
I want to use TPS2051 in an USB OTG application.
When configured as Device the USB Power is supplied from the USB Connector and the TPS2051C is disabled.
When the…
Other Parts Discussed in Thread: TPS2051C Please teach me two questions about TPS2051C.
1, I cannot find 「continuous Power Dissipation」 in datasheet.
My customer needs this information.
2, Please teach me thermal shutdown operation detail. …
Part Number: TPS2051C Dear Specialists,
MY customer is encountering the broken issue of TPS2051C and investigating.
Could you please confirm the condition whether there is a problem.
---used case
When Vin is VBUS(5V), 6V( a few ms width) is added…
Other Parts Discussed in Thread: TPS2051C , TPS2041C Hi all, Would you mind if we ask TPS2041C, TPS2051C? <Q1> The datasheet shows "Additionally, bypassing the output with a 0.01-μF to 0.1-μF ceramic capacitor improves the immunity of the device to short…
Other Parts Discussed in Thread: TPS2553 , TPS2051C Hello there,
I wanted to get some clarification on the TPS2051C and it's ability to cycle on and off during a heavy-overload or short-circuit event, it sounds very much like the "auto-retry" non…
Other Parts Discussed in Thread: TPS2051C Couly you please let me know what is the typical Rds(on) of TPS2051C at the following conditions:
Vin=5V and Iout=50mA,
Vin=5V and Iout=100mA
Vin=Ven
preferrably for –40°C ≤ T J ≤ 125°C
thank you
Other Parts Discussed in Thread: TPS2051C Hi,
Contradictory statements are found for output capacitor of TPS2051c:
On datasheet SLVSAU6G page 16, “Typically a 150 μF electrolytic capacitor is used”.
On SLVU466B EVM BOM, 150 μF C4 is tantalum.…