Part Number: TPS2052B Hi, we are using only one output. EN2=GND. We expected a current limit with < 1.3A max at the output or typ. 1A, but we are measuring 1.53A. I read in another task that this part has flat current limit. TPS20x1B and TPS20x2B devices…
Part Number: TPS2052B Tool/software: Do you know id the TPS2052BDGNRG4 life cycle is Active & i know the TPS2052BDGNR IS ACTIVE but not the TPS2052BDGN JUNE 5 2025 IS OBSOLETE.
Part Number: TPS2052B I have attached the schematics for the IC TPS2502B, could you please review this?. I was facing a back drive issue on OUT1 and OUT2 which i have used for HDMI. So there was a path from OUT to IN due to which i was facing a back drive…
Part Number: TPS2052B
Dear Team,
Could you please check whether if the output pin of the TPS2052BDGNR gets a voltage back will that IC will be able to supress that and will that be back driven to input. Like I will be using the output to give supply…
Part Number: TPS2052B Tool/software: Dear Team,
I have attached the power logic pdf using TPS2052BDGNR, can you please verify this.
Ti Logic IC PRJCL-02.pdf
Thanks, Irfan
Part Number: TPS2052B Other Parts Discussed in Thread: TPS2561 Tool/software: Dear Team,
I am designing the HDMI Interface where my one connector acts as both input and output and as per HDMI the voltage 5V will sink to my board if it acts as input…
Part Number: TPS2052B Tool/software: Dear Team,
I need to know the reflow soldering profile for TPS2052BDGNR. Request you to share the graph of it.
Regards, Irfan
Part Number: TPS2052B Hi TI team,
Iam using #TPS2052B power switch for 2 PCBs to acesss /connect USB devices (Pen drive) .
PCB 1 Design : by using TPS2052B switch Iam made acees two USB ports and below is the circuit.
PCB-2 Design:
#TPS2052B…
Part Number: TPS2052B Tool/software: Dear Team,
In TPS2052BDGN when the EN receives the input high what time does it take to give the output. I wanted this because I am enabling 2 different IC with same enable so i want the output time required.
Regards…
Part Number: TPS2052B Tool/software: Hello,
My customer has been using TPS2052BDR for a long time. They would like to get the details of the following specification revisions in the TPS2052B datasheet history.
Could you please provide details of the…