Part Number: TPS2065C-2 Hello Expert,
I need CB, UL (IEC62368-1) Certified Report.
Could you send it to me by e-mail?
michael.jeong@arrow.com
Best regards,
Michael
Part Number: TPS2065C-2 Vin min is 4.5V Vuvlo is 3.75Vtyp
If Vin is, for example 4.1V, what will happen if nEN is 4.1V? Will the output be fully off? This is the scenario I'm hoping.
I need to know if the part will appear off if the nEN is pulled…
Part Number: TPS2065C-2 Other Parts Discussed in Thread: TPS2065C ,
Hi Team, My customer considers to use VBUS switch for USB Downstream Facing Port. I saw there is device with output discharge as TPS2065C and without as TPS2065C-2. Is the device with…
Part Number: TPS2065C-2 Hi,
We got a question from the customer about TPS2065C-2. Could you help us?
[Question] When VIN and EN voltage disappears, the voltage of VOUT exists due to the charge voltage of super capacitor. Are there any concerns on…
Part Number: TPS2065C-2 Other Parts Discussed in Thread: TPS2065C Hi Team,
Could you please check the connection of TPS2065CDBVR.
It is ok to connect FLT pin to EN pin (IO from MCU) with 100 Ohm resistor?
The resistor between pin 5 and 1 is option…
Hi Frank,
They are looking for something similar to page 43 of the TPS2065C-2 datasheet: http://www.ti.com/lit/ds/symlink/tps2065c-2.pdf . This DGN package seems to have a slightly different PowerPad PCB land pattern so I wanted to check if there's…
The TPS2041C will not conduct current from OUT to IN when IN is unpowered. If IN is powered, pulling /EN high will also disable reverse current. However, when disabled with the input powered, an output discharge will draw current. Within the "C" family…
Hello MJ,
The ESD ratings shown in the TPS2065C datasheet cannot be applied to surges as they are different; surges can be up to 200 times the length of an ESD event (based on the waveform models of the IEC 61000-4-2). Due to the longer pulse length…