Hi Michael,
Thanks for your swift response. Could you help me to understand the following questions:
(1) Since there's no protection for this case. Will this damage the device if Vin always stay at 5V and Vout always at 5.14V or 5.5V? (2) Any reverse…
Part Number: TPS2065C Other Parts Discussed in Thread: TPS2069C , TPS2051 Dear expert,
Basically i want to power on the BBB with 5V 2.5A
because i need 1.5A power on USB port
hence i decided to make custom BBB it will exactly same as current BBB with a…
Part Number: TPS2065C Other Parts Discussed in Thread: TPS2553 , TPS2069C Good day Colleagues,
My customer uses the TPS2065CDGNR but claims the Ron resistance is 2 times higher than a datasheet described.
He measured voltage drop with a resistive load …
The TPS2041C will not conduct current from OUT to IN when IN is unpowered. If IN is powered, pulling /EN high will also disable reverse current. However, when disabled with the input powered, an output discharge will draw current. Within the "C" family…