Part Number: TPS2066 Hi
Could you tell us the difference between TPS2066DGNR-1 and TPS2066DR?
I think TPS2066-1 has discharge control, but TPS2066 is not..
Could you please point out the difference between TPS2066-1 and TPS2066?
BestRegards
Part Number: TPS2066 Hi,
We are currently using the TPS2066D as load switch for USB ports. y at the VIN pin ramps up, a glitch occurs on the OC# pin while VIN is still very low (~ 0.72V). This glitch is sometimes interpreted as an overcurrent event by…
Part Number: TPS2066 Hi, Could you tell me about TPS2066 EN pin? The TPS2066 Enable pins (EN1 & EN2) are active high. If I want to permanently enable the outputs I would pull these pins high to 5V. In this case should I use a pull-up resistor i.e. 10kohm…
Part Number: TPS2066 HI,
I am considering the following contents in performance evaluation. It is shown in the figure. Is it OK to apply voltage externally to OUT pin with voltage applied to IN? EN turns it off. If the voltage at OUT is higher than the voltage…
Other Parts Discussed in Thread: TPS2066 The TPS2066 Enable pins (EN1 & EN2) are active high. If I want to permanently enable the outputs I would pull these pins high to 5V. In this case should I use a pull-up resistor i.e. 10kohm?
Hi Sirs,
Sorry to bother you, could you please help to suggest output load cap value?
Because we have use 470uF, but looks the IC doesn't work.
At data sheet fig 7(page 10), we think 470 uF should be OK.
Need your help to clear our question. Many…
Hi
we are using TPS2066DGNG4 load switch in our design,but the chips fails in some of the boards. During the board bring up and functional test it was working fine, but it failed on some of the boards during field testing. While we analaysed the failed…
Part Number: TPS2066C Other Parts Discussed in Thread: TPS2066 , Hi Team,
How about TPS2066 IEC62368-1 3rd CB report status in the now?
Best regards,
Sato
Other Parts Discussed in Thread: TPS2066-1 Dear Darwin-san and Sir
I'm really afraid again . About TPS2066-1 (TPS2066DGNR-1) 's certifiation ,
We talked with our customer about CB TEST and certification.
Customer need not only CB test and certifications…