Hi Praveen,
The power supply is about 200cm from the IC, and I add the capacitor close to the vcc pin of TPS24701(parallel with c133, c147(10uF)is the capcitor that I added). When I test the waveform, I added a 30ohm resistor (R458) to GND behind the…
Part Number: TUSB8042A Other Parts Discussed in Thread: TPS2066 , TUSB8020BEVM Hi,
Please find the schematic in the link below.
https://e2e.ti.com/support/interface/f/138/t/895306
Issue:
PWRON1_BATEN1,PWRON1_BATEN2 act as low level and can't enable the…
Part Number: TPS2066 I am using TPS2066 for power sequencing purpose., the switch is being used to generate two voltages namely SSD_3.3V & EX_3.3V.
SSD_3.3V is Voltage for M2.SATA
Ex_3.3V are peripherals of processor
1. It is found that in some cases…
Hi, Taemin,
There shows 3 kinds of ESD protection level.
1. HBM(human body model)
2. CDM(charge device model)
3.IEC 61000-4-2. It includes contact discharge and air discharge.
From datasheet, TPS2066 and TS3USB3000 just support HBM and CDM level ESD…