Part Number: TPS22902 Hi Team,
We are using the TPS22902YFPR Load switch part in our schematics. I had attached the schematic Image below, Kindly review the schematics and share your valuable feedback with us.
Thanks and Regards
- Teja
Dear TI Team,
I have go through one Application Report SLVA670A for the inrush current due to capacitance.
my question is that how measure the Inrush current(3.12A) value in below image.
if i am using the formulae which is given in the Application…
Part Number: TPS22902 Other Parts Discussed in Thread: TPS22916 Dear all,
I'm migrating a design from a TPS22916 (currently not available) to a TPS22902. It is used to power a 3.3 V NOR flash memory. The TPS22916 has a pull-down resistor at the ON pin…
Part Number: TPS22902 [
urgent]Please let me know the position of first pin in the actual sample. TPS22902YFPR.
We attached the figure. Please mark around the first pin. A1 and B1.
Part Number: TPS22902 Hi expert,
Customer is asking IEC 62368/EN 62368/UL 62368 spec for TPS22902YFPR. Do we have data could provide to them? Thanks!
Best regards,
Ann Lien
Part Number: TPS22902 Dear Specialists,
My customer is evaluating TPS22902YFPR and encountering problem.
Could you please advise?
---questions
I am evaluating TPS22902YFPR, some samples are not working correctly.
When the device is power ON…
Other Parts Discussed in Thread: TPS22902 Hi Team!
I am looking at the TPS22902 and want to find the landing pattern for this. I looked at the datasheet and could only find the mechanical drawing. However, I do not see one available. Am I missing something…
Part Number: TPS22901 Other Parts Discussed in Thread: TPS22902 , TPS7A02 1) What issues would we face if Cout/CL (capacitance at output side/load side) is more than Cin in TPS22901 resulting in a condition of Vout>0 when the power source is removed.…
Part Number: MSP430FR2433 Other Parts Discussed in Thread: TPS22902 , Hi,
I have a customer that is using the MSP430FR2433, but they are also using a load switch [TPS22902 (tr = 40 us) or potentially the TPS22902B (tr = 200 us)] in front of it to control…