Other Parts Discussed in Thread: TPS22946 We are using the TPS22946 to switch +5Vdc to optical detector IC ( Iload=10mA )
We found out that the device does not start sometime ( very random ) !
The circuit is connected with 'CL' and 'ON' are tied to Vin…
Other Parts Discussed in Thread: TPS22946
I do not see a spec on trip-point hysteresis. Im trying to find out how the parts behaves with a very gradual load increase that may be noisy. Once the part senses a slight overcurrent condition, how much does…
Part Number: ADS114S08 Other Parts Discussed in Thread: TPS22946 Hi here is a quick overview of the system. I am designing a battery powered prototype of potentiometer(s) readout. The device displays the potentiometer wipers ratio value in an LCD and goes…
David,
We have /some/ load switches that might work for you as long as your current is <500mA DC.
I would recommend to look at TPS22946 and TPS22951
They have either selectable or fixed current limits and are 5.5V max VIN parts. They are also available…
Hi Alek,
TPS2595 and other eFuses seem to have much higher Iq than TPS2294x. Indeed, TPS22946 seem to be better but the only drawback is that it is BGA package.
Can you suggest whether I should be checking in any other forum for getting a closest matching…
Other Parts Discussed in Thread: TPS22946 , TPS22918 Hola,
I wanted to ask someone if you have a power switch similar to TPS22946.
http://www.ti.com/lit/ds/symlink/tps22946.pdf
But our requirement is input/output voltage is 1.8V and the maximum current…
Other Parts Discussed in Thread: TPS22951 , TPS22946 Hi all. My customer would like to evaluate TPS22951, but I don't get the EVM of TPS22951. Does this device have EVM? If this device doesn't have EVM, do you have instead of the EVM? Best Regards, …
Alexander,
Our Universal Search on has Cross References built in. I just plugged this device into our Cross Reference Search and it shows the TPS22946 and TPS22951 have the same functionality.
Here is a link to the search results/cross reference: http:/…
Other Parts Discussed in Thread: TLC59108F , TPS22946 Hi, we want to use the TLC59108F. The datasheet does show: Low Standby Current.
How big is this standby current? Is this current active, when all LEDs are off (6 mA / 3V) or can I reduce this current…
Hi Alex,
Have you been able to confirm the TPS22946 will work for your design?
Best Regards,
Adam
___________________________________________________________
If all your questions have been answered, please login & click Verify Answer on those…