Hi Kaknevicius:
Thanks for your suggestion, but TPS22951 continues current spec:300mA.
Since my application continues current need 350mA.
Do you have other suitable solution that continues current spec around 500mA?
Looking forward your reply, thanks…
Hi Suman,
With a 3.3V voltage and a 7 ohm load, your current would be about 470mA. The TPS22951 has a current limit of 600mA and can support voltages between 2.2V and 5.3V. Please let me know if this load switch would fit your needs.
Regards,
Alek Ka…
Alexander,
Our Universal Search on has Cross References built in. I just plugged this device into our Cross Reference Search and it shows the TPS22946 and TPS22951 have the same functionality.
Here is a link to the search results/cross reference: http:/…