Part Number: TPS22993 Hi,
How to set eight I2C unique address for our TPS22993?
Our system needs eight TPS22993 to do configuration. but the TPS22993 only have 7 unique I2C address.
any suggestion?
Part Number: TPS22993 Tool/software: Hi TIer
Do we have 8 channel load switch?
What is the difference between the load switch and the high side switch or the low side switch?
Thank you very much.
Part Number: TPS22993 Other Parts Discussed in Thread: TPS22810 , TPS4H160-Q1 Hi team,
I 'd like to select a high Vds(>10V) load switches which have at least four channels. Could you recommend the proper device?
Thanks in advance!
Part Number: TPS22993 Other Parts Discussed in Thread: USB2ANY Hello,
I am using TPS22993EVM-033 and USB2ANY. After the I2C Load Switch Device GUI is started there is no USB 3.3V and USB 5V on the evaluation board (jumpers are set for USB voltage…
Hi Michael,
I tested this in the lab today and found that the load switch functioned properly (with GPIO control) when VDD was left floating.
Thanks,
Alek Kaknevicius
If the power up sequence of I2C has conditions, please let me know.
・After VDD (or Vbias) rise, in how many times does I2C start?
・After I2C start, in how many times until the device operates?
・What operation is I2C not able to be read?
(Is there…
Part Number: TPS2054B Other Parts Discussed in Thread: TPS2044B , , TPS22993 , TPS22994 I am looking for USB Power Switches which have four channels and Continuous current (max) (A) above 0.5A and upto 1A.
Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: LM3880 , TPS22993 Hi Team,
Can you suggest a power management module that would allow the user to enter/exit the sleep mode feature of the phy ethernet DP83TG720S-Q1?
Can you confirm the…
Hi Salyali,
What sort of functionality are you looking to program? In general, these are pretty simple devices, but the TPS22993 can be programmed through I2C.
Thanks,
Alek Kaknevicius