Part Number: TPS23750EVM-108 Other Parts Discussed in Thread: TPS23750 Hi all,
We observed a R13 resistor value difference between TPS23750 datasheet and flyback EVM for 5V output.
In datasheet value mentioned is 10K & in EVM it is mentioned as…
Part Number: TPS23750EVM-108 We have a product which has POE as its main power supply. It is used as a gateway between internet and a local 868 MHz network. The current POE components we have used are no longer available, so we have redesigned this product…
Part Number: TPS23750EVM-108 Other Parts Discussed in Thread: TPS23750 , TPS23755 , TPS23753A , TPS23758 , PMP8803 , TPS23755EVM-894 , TPS23753 I have TPS23750 Flyback-Converter Evaluation Board(HPA108).
This Board is 3.3V Output. I woud like to change…
Part Number: TPS23750EVM-108 In SLUA469 it is discussed how to fight down conducted emissions by adding a CM choke (Pulse PE-53913NL). However, the referred eval board (TPS23750EVM-108) does not look the same as the one discussed in SLUA469. I do not…
Part Number: TPS23750EVM-108 Other Parts Discussed in Thread: STRIKE In the case of an isolated design; How is an ESD spark on the secondary side handled by the circuit? I assume the gnd of the secondary side is connected to the chassis. Thus, when an…
Hi Shinichi,
If ou change your your optocoupler, you should change R12 and R24 in TPS23750EVM-108.
below is the equation can help you to find the right components value.
-Ben
If this post answered your question, please click Verify Answer…
Hi Benjamin,
This EVM is only released with the 3.3V version. Modification to a 5V rail is fairly simple. Looking at the user's guide BOM, you only have to replace R12, R13, R18, R19, R20, and T2 with those components specified in the -002 BOM. Below…
Other Parts Discussed in Thread: TPS23750EVM-108 , TPS23750 Hello Support.
Could you recommend another one popular T2 transformer which used in your TPS23750EVM-108 (for 3.3v version)? It is looks like End of Life.
TPS23750 is a still Active ? Or…