Part Number: TPS23750EVM-108 Other Parts Discussed in Thread: TPS23750 Hi all,
We observed a R13 resistor value difference between TPS23750 datasheet and flyback EVM for 5V output.
In datasheet value mentioned is 10K & in EVM it is mentioned as 1.5K.…
Part Number: TPS23750EVM-108 We have a product which has POE as its main power supply. It is used as a gateway between internet and a local 868 MHz network. The current POE components we have used are no longer available, so we have redesigned this product…
Part Number: TPS23750EVM-108 Other Parts Discussed in Thread: TPS23750 , TPS23755 , TPS23753A , TPS23758 , PMP8803 , TPS23755EVM-894 , TPS23753 I have TPS23750 Flyback-Converter Evaluation Board(HPA108).
This Board is 3.3V Output. I woud like to change 12V output…
Part Number: TPS23750EVM-108 In SLUA469 it is discussed how to fight down conducted emissions by adding a CM choke (Pulse PE-53913NL). However, the referred eval board (TPS23750EVM-108) does not look the same as the one discussed in SLUA469. I do not see…
Part Number: TPS23750EVM-108 Other Parts Discussed in Thread: STRIKE In the case of an isolated design; How is an ESD spark on the secondary side handled by the circuit? I assume the gnd of the secondary side is connected to the chassis. Thus, when an…
Other Parts Discussed in Thread: TPS23750EVM-108 Dear Specialists,
My customer is confirming TPS23750EVM-108.
When an Optocoupler was only changed, the board wasn't work well.
The Optocoupler is from TCMT1107(original) to PS2801C-1.
I couldn't find…
Hi Benjamin,
This EVM is only released with the 3.3V version. Modification to a 5V rail is fairly simple. Looking at the user's guide BOM, you only have to replace R12, R13, R18, R19, R20, and T2 with those components specified in the -002 BOM. Below…
Other Parts Discussed in Thread: TPS23750EVM-108 , TPS23750 Hello Support.
Could you recommend another one popular T2 transformer which used in your TPS23750EVM-108 (for 3.3v version)? It is looks like End of Life.
TPS23750 is a still Active ? Or maybe…