Part Number: TPS2511 Hi Team,
The ILIM_SET is 2A (Riset is 24.9K), but Android phone and I phone can only sink 0.8A, and IPAD can only sink 1.3A.
Our customer use original cable, and the voltage at TPS2511 OUT is 5.5V.
Please help to check this, thank…
Part Number: TPS2511-Q1 Hi Team
My customer has question about TPS2511-Q1 again.
TPS2511-Q1 has two internal FET . Typically each FET has body diode.
Let me know body diode max Repetitive peak reverse voltage(Vrrm) , max Forward rms current(If) and Ma…
Part Number: TPS2511-Q1 Hi Team.
My customer has a question about TPS2511-Q1.
TPS2511-Q1 has specification about continuous output source current (=ILIM_SET)
but, No Maximum output current of OUT
Let me know Maximum output current and time.
Thank you…
Part Number: TPS2511-Q1 Other Parts Discussed in Thread: TPS2549-Q1 , TPS25810A-Q1 , TPS254900-Q1 Dear All
Can the TPS2511-Q1 device support to MFi (Made For iPhone/iPod/iPad) certification ?
And there are other device can elso support MFi ?
Thanks. …
Part Number: TPS2511 Hi,
For a new product we need to implement a DCP charger and I was considering the use of the TPS2511 to have peace of mind as regards to connectivity to various phones and tablets. My question is regrading the current limit. The…
Part Number: TPS2511 Other Parts Discussed in Thread: TPS2546 Hello E2E,
During operation, when not connected USB connector that how much the voltage for D+/- port?
Regards,
ACGUY
Part Number: TPS2511-Q1 Other Parts Discussed in Thread: TPS2553 , TPS25221 Hello,
Can TPS2511-Q1 be used with D+/D- unused?
My customer is considering using it as a simple USB switch, because it is the cheapest USB switch with adjustable current limit…
Part Number: TPS2511
Hello We have a product that has two usb ports and we are thinking to use two TPS2511. But what if we use only one control charger with two usb ports in parallel connected with data line + and -. What problems can we have if in usb…
Part Number: TPS2511 Other Parts Discussed in Thread: TPD1E10B06 Team,
I have some question regarding TPS2511 as below.
1. If they are not using /CS, then it can be leave open?
2. when they set I_limt=1.5A, current will flow up to 1.5A or shut down the…