Part Number: TPS2511
Hello We have a product that has two usb ports and we are thinking to use two TPS2511. But what if we use only one control charger with two usb ports in parallel connected with data line + and -. What problems can we have if in usb…
Part Number: TPS2511 Other Parts Discussed in Thread: TPD1E10B06 Team,
I have some question regarding TPS2511 as below.
1. If they are not using /CS, then it can be leave open?
2. when they set I_limt=1.5A, current will flow up to 1.5A or shut down the…
Part Number: PMP8363 Hi,
I have a quesion about the schematic of the second circuit, the last part with the resistor net (R2-6). What values here and also aren´t you using the TPS2511? How to you connect this in to the cirucit since it must have…
Part Number: TPS2511-Q1 I'm currently testing a circuit that includes the TPS2511QDGNRQ1 USB Dedicated Charging Port Controller and Current Limiting Power Switch. The documentation says that the values for D+ and D- should be one of the values: 2.0V…
Part Number: TPS2511-Q1 Other Parts Discussed in Thread: TPS2511 Dear Greetings,
I am examining TPS2511-Q1 for USB charger of vehicle.
I have some questions.
1. When I checked EVM, Rilim is applied 1/10W(1608 size).
Should I apply 1608 size for Rilim…
Part Number: TPS2511 Hello Team,
Can the TPS2511 in unpowered state (no input voltage at IN pin) be damaged by applying USB On-The-GO Service Request Protocol (voltage pulses on V_bus and USB data lines) at the output of TPS2511, please ?
USB OTG multi…
Part Number: TPS2511-Q1 Other Parts Discussed in Thread: TPS2511 H
There are the description to place a via in center of solder mask in TPS2511-Q1's datasheet. However my customer need good radiation. So they place four via as attached document. Are…
Part Number: TPS2511 Hi Team,
My customer evaluating our TPS2511 and performing a DCP test using TPS2511EVM. However, they couldn't pass the test.
See attach the setup (putting 12V power supply to the input, and tested with MQP pocket master USB PET…