Other Parts Discussed in Thread: TPS2513 , TPS2513A Hello,
TPS2513 supports dedicated charging port Auto detect mode, DCP Divider 1(5 W) and Divider 2(10W). TPS2513A supports dedicated charging port Divider mode 3(12W).
My questions are:-
1) I have a…
Other Parts Discussed in Thread: TPS2513 , TPS2561 , TPS2511 , TPS2513A My 1 st question is: what benefit(s) are there (or maybe just differences) in implementing a USB charging circuit using the TI parts: TPS2561 and TPS2513 to support a dual USB charger…
Other Parts Discussed in Thread: TPS2511 Hi there,
Quick question other than the dual channel what are the differences between the above. I currently have a product that is using 2x TPS2511 as Dedicated Charger and I came across the 2513 that has both…
Hello Cory,
TPS65988 does have a register that can read the current that is currently sourced from the device. The amount of current pulled is determined by the downstream device. The BC1.2 advertisement only advertise the maximum current supported by…
Hi Ricardo,
This does help some. The forum does provide some info on divider 1, 2, and 3. It is sprinkled throughout multiple posts, which is not ideal, although this did lead me to look at the datasheet for the device they are discussing: www.ti.com…
Part Number: TPS2513A-Q1 Other Parts Discussed in Thread: TPS2513 I have been working with the TPS2513 to provide data signatures to a charging-only USB port. The chip has been working normally and providing the correct signatures for charging. However…
Part Number: TPS2561A-Q1 Other Parts Discussed in Thread: TPS2513 , TPS2561 I have been working with the TPS2513 and TPS2561 for wiring a USB port. However, I am having some trouble getting the output voltage that I want while staying within the 7V maximum…
Part Number: TPS2561A-Q1 Other Parts Discussed in Thread: TPS2561 , TPS2513 I am trying to run simulations on the TPS2561 and TPS2513 using the TINA software. However, when I compile the imported PSpice netlist for these components, it gives me the error…
Hi Nathan,
TPS2513 is support DCP auto charging for iphone and sumsung phone. If you just need charging function for the phone , the tps2513 is suitable for your solution.
TPs2513 is focus on charging whithout data communication in the DP/DM line. If…
Hi ,
I think you are want to use tps2513 and tps2561 to configure a charging only USB port.
If that , you can let the other pin floating , the floating pin will not impact the charging port you design.