Part Number: TPS2547 Tool/software: Hi AE,
Currently, The Type-C port with BC1.2 via TPS2547 and the CC pins handled by a CC controller for Type-C protocol.
We support 5V3A
Current testing on the iPhone 15 shows different results between DCP and…
Part Number: AM623 Other Parts Discussed in Thread: TPS2547 , We have a design leveraging a AM623 that leverages USB0 boot via DFU. USB0 passes through a TPS2547 before reaching the USB connector. We are experiencing an issue where it appears the USB…
Part Number: TPS2547 Other Parts Discussed in Thread: TPS2546 Tool/software: Hello,
I understand that the TPS2546 implements CDP-SDP auto switch functionality, while TPS2547 does not.
My question is - what implications would the TPS2547 not implementing…
Part Number: TPS2547 Other Parts Discussed in Thread: BQ24392 , TPS2546 , Tool/software: Hi team,
BQ24392, BC1.2 detector cannot pass BC1.2 compliance test.
TPS2547 or TPS2546 can replace BQ24392? and these device can pass BC1.2 compliance test…
Part Number: TPS2547 I want to double confirm that whether TPS2547 support 5V 2.4A. (Apple)
In the datasheet, it seems only support 5V 1A and 5V 2.1A. (Apple)
Is it right?
Part Number: TPS2547 Other Parts Discussed in Thread: TPS2546 , TPS2549 , TPS2544 Hi
Customer would like to evaluate 2547 to replace 2546, and from datasheet, tps2547 is drop in BOM compatible with tps2546.
Compare with spec,
1. 2547 remove…
Part Number: TPS2547 Hi Team,
Customer put forward a new question about TPS2547.
At the NB S0 state, they will config CDP mode. When NB change to S3 state, they will be config SPD mode. The found the Vout will be drop. Is this normal performance?…
Part Number: TPS2547 Other Parts Discussed in Thread: TPD4S014 , TPD4S214 Hi Team,
Customer is wondering if they need to add a OVP(in case end user add a >5V source) at our TPS2547 output side, how to protect it ?
Clamping Diode or OVP part ?
…
Part Number: TPS2547 Other Parts Discussed in Thread: TPS2546 , , TPS2544 Hi, USB Power Switch support team
I understand that there are the difference point as the following table.
As for the feature except the above I would like know if it is backward…
Part Number: TPS2547 Hi team,
Does TPS2547 support below requirements?
- Can detect STD
- Can detect USB 1.2 STD DCP and CDp
- no USB PD
- Don't need to use I2C
Are there other recommendatons?
Best regards, Shunsuke Yamamoto