Part Number: TPS2553-1 Hello,
I would like to know if Texas Instruments provides any MTBF or FIT data for the device TPS2553DBVR-1.
The device is used under continuous operation at an ambient temperature of 70 °C.
If no part-specific MTBF…
Part Number: TPS2553-1 Tool/software: I’m currently qualifying the TPS2553DBVT-1 as part of a preliminary risk assessment and I’m looking for information regarding its fabrication process.
I couldn’t find any PCN related to this part, and the available…
Part Number: TPS2553-1 Tool/software: Hello E2E Experts,
Good day.
I chose the latch-off model. But when a short circuit occurs, the fault output switches from high to low and then back to high (and does not stay low all the time), even if a short…
Part Number: TPS2553-1 Hi Sir,
Please refer to the below scope waveform and the schematic.
When the system power-off, if the output cap(C431) does not fully discharged, the TPS2553-1 will go to Reverse-Voltage Protection mode and asserts the FAULT…
Part Number: TPS2552-1 Other Parts Discussed in Thread: TPS2553-1 , TPS2553-Q1 , TPS2553 , TPS2552 Hello guys,
I have seen that the model TPS2552-1 is very similar to the TPS2553-1 (only enable pin is different) but there is no automotive version…
Part Number: TPS2553-1 Hello Sir:
We studied the datasheet and found below descriptions.
"The device remains off regardless of whether the overload condition is removed from the output. The latch-off devices remain off and do not resume normal operation…
Ziv Zhang said:
Hi Gokhan,
TPS2553-1 is latch off version. TPS2553 is constant current limit version.
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help…
Part Number: TPS2553-1 Hi
My customer use TPS2553-1×2pcs in parallel to control 2 input.
I think that this using method are no problems if one device is disabled.
If two devices are ON at a time, are there the problems?
Best regards, …
Part Number: TPS2553-1 Other Parts Discussed in Thread: TPS2553 Hi team,
Can TPS2553-1 be used in below circuit for auto retry function?
In my opinion, I don't think it can work like TPS2553 since in latch mode, the fault will be always low during…