Hi Hirokazu,
In datasheet TPS2557, Page7, Fig2 can answer your question.
If toff=6ms, as EN go low 3ms, the part will still keep on status for another 3ms.
Noted, Page7, Fig2 is TPS2556 which turns on as low EN.
Other Parts Discussed in Thread: TPS2546 , TPS2556 , TPS25200 , TPS2549 Hi Team,
I am just wondering that whether or not TPS2546 can avoid the back-drive issue from external device ? or we need to add another IC to prevent it. Please advised.
Thanks,
Leroy…
it looks like the peak current is 3.3 A. I think that may be beyond the current limit, causing your voltage to drop. The TPS2556 current limit is set to 1 A though. I wonder where the extra current is going? I would suggest that you discinnect the…
Other Parts Discussed in Thread: TPS2561A-Q1 , TPS2561-Q1 , TPS2556 Hi,
I would like to know how to design the input/output capacitor of TPS2561A-Q1.
Though there is no mention about the input/output capacitance on the datasheet of TPS2561A-Q1.
There is…
David,
Echo to Eric, addtionally:
If you need 2.4A charging spec, you can use TPS2514 A +TPS2556/7.
TPS2514A supports the new 2.4A iPad charging spec. ANd TPS2556/7 has the extra low Rdson 22mohm and very accurate current limit.
No, for TPS2546, all the DCP_Auto modes' current limit depends on ILIM_HI. Maybe you can configure two-level current limit refer to Figure 22 on page 15 of TPS2556 for the DCP_Auto mode.
How about 2 x TPS2511, Figure 35 and 37 on page 20, one port…
Thanks John for the reply. Yes we're talking about the TI ref design. We're trying to build a 12.5W 5V, 2.5A USB charger using the same IC. Can we use the 'Renco transformers- RTLI-1061 or 1067' for this design of 12.5W load using the…
Other Parts Discussed in Thread: TINA-TI Update of TINA9-TI Spice Model Libraries and Example Circuits
This note describes the step-by-step process for updating the TINA9-TI Spice Macro Libraries and Example circuits. The update is initiated by selecting…