Part Number: TPS2561 I design set-top box have USB port
TPS2561 is designed for USB, and for IEC62386-1 certification.( US-37138-UL)
But TPS2561 doesn't have Input Over Voltage LockOut(or Clamping).
How certificate IEC62386-1 with TPS2561?
Is…
Part Number: TPS2561 Hi Sir,
I tested TPS2561 with different current limit setting and got abnormal behavior when over current occur.
For 1.4A current limit, TPS2561 is auto retry when OC occur; but for 1A current limit setting, TPS2561 isn't auto…
Part Number: TPS2561 Hello,
I have used the TI TPS2561 current limited power switch on two different designs.
It has worked well for me using the switch on a four port USB Hub with a Panasonic NN31001A-BB DC/DC converter switching at 800kHZ .
However…
Part Number: TPS2561A Other Parts Discussed in Thread: TPS2560 https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/350238/what-is-the-difference-between-the-tps2561-and-tps2561a
The explanation of Milo is still…
Part Number: TPS2561 Hi,
I only want to use Channel 1 on this part. How do you disable EN2?
Do I tie EN2, Fault2 and OUT2 to GND? Or, do I leave them unconnected?
Part Number: TPS2561 My customer is asking following number to complete their system design.
Is there certification number of TPS2561 for TUV(European certification ) similar to IEC 60950-1 ?
If not for TPS2561, could you tell us alternative device…
Part Number: TPS2561 Other Parts Discussed in Thread: TPS2560 Hello Expert,
I have a question.
Is there internal Pull-up or Pull-down resistor in EN pin which is TPS2561, TPS2560?
If yes, what's the resistor value?
Best regards,
Michael
Part Number: TPS2561 We are currently using a TPS2561DR in our design; however due to this part being out of stock with a long lead time, we are looking for a direct part swap. This part is being used to limit power current of USB and SATA power supplies…
Part Number: TPS2561 Hi,
I am only using channel 1 on the TP2561 for power management for a USB port. I want to disable the second channel as it is not being used. Do need to connect EN2, Fault 2 and Out2 to GND? Or, do I leave them unconnected?
Regards…