Part Number: TPS25810-Q1 Other Parts Discussed in Thread: TPS25810
Hi,
I would like to know behavior of the TPS25810-Q1 duirng in the case of reverse voltage condition.
For instance, the case is that mobile battery 5.2V is connected with output when…
Part Number: TPS25810-Q1 Other Parts Discussed in Thread: TPS25810 Hi,
If repeating current limit condition many times, is there any possibility to damage for the TPS25810-Q1?
Best regards,
Kuramochi
Part Number: TPS25810-Q1 Hi,
If the TPS25810-Q1 is located into thermal shutdown condition during long term(1000h), is the TPS25810-Q1 damaged?
Thermal shutdown condition means that repeating thermal shutdown and restart.
Best Regards,
Kuramochi
Part Number: TPS25810-Q1 Hi,
We got a question from the customer about TPS25810-Q1. Could you help us?
[Question] Are there any input and shutdown sequence requirements between following pins?
INx AUX EN CHG CHG_HI
Best Regards, tateo
Part Number: TPS25810-Q1 Other Parts Discussed in Thread: TPS25810A-Q1 , TPS25810 , Hi,
Ios is specified on Rref=10Ω as below.
Though Rref must be set to 10kΩ basically, what case is this specification supposed?
Best Regards,
Kuramochi
Part Number: TPS25810A-Q1 Other Parts Discussed in Thread: TPS25810-Q1 , , TPS2514A-Q1 Hi,
Except for except for blocks which are different specification as below, are TPS25810A-Q1 chip and TPS25810-Q1 common chip?
e2e.ti.com/.../669445
Best Regards,
K…
Part Number: TPS25810-Q1
Hi,
I think that the current limit value is varies by Rref.
Could you show me the equation to calculate the valuation of current limit by Rref on the 1.5A mode and 3A mode?
Best Regards,
Kuramochi
Part Number: TPS25810A-Q1 Other Parts Discussed in Thread: TPS25810-Q1 ,
Hi,
I heard that UVLO is different during TPS25810-Q1 and TPS25810A-Q1 on the following thread.
However I couldn't find the difference.
Q1. What is the difference of UVLO during…