Hi Shubha
Could I get any update wuth this? Should I file another ticket to get the answer?
The part TPS25821 development is work in progress.
Please help to support.
Look foeward to your responds.
Hi Gary ,
Apologies for the delay.
Please find my comments below -
1. Connect a 0.5%, 100-ppm, 100-kΩ resistor between this pin and GND. Make sure tolerance is 0.5%.
2. Capacitance at OUT is not clear in the schematic. Make sure it is at least 0.1uF. …
Hi,
TPS25821 and all our devices are designed to meet the spec of USB2 and USB3.
Does your customer plan on applying for any certification or pass any compliance? Limiting the the current to 500mA for USB3.1 will not pass the compliance.
If your customer…
Part Number: TPS25821 Other Parts Discussed in Thread: TPS2553 , Hello TI Team,
I have requirement to design source only USB Type-C port which will only source VBUS (5V ) supply with aprx. current 1A.
I was come across TPS25821 and TPS2553 Power switches…
Part Number: TPS25821 Hi team,
My customer would like to confirm with you about the CHG function as below. Thanks.
So for our design, should we let CHG to low? But how to know that is USB2.0/3.1 port?
If the condition is CHG 0, and STD(500mA for USB…
Part Number: TPS25821 Hello Team,
I am working on Source only USB-Type C application. I am considering TPS25821 as power switch.
I was going through schematic of reference design PMP40270 where 200Ohm (R6 ) is used.
Please can you explain what is the use…
Part Number: TPS25821
Hi team,
I help customer to ask a question.
" Test three pieces of bad output The first piece of output is not normal in less than one second The second piece has no output The output of the third piece is only 2V After yesterday…
Hi Rain,
One issue with using two separate USB 3.0 ports for a single Type-C port, is that if a USB 3.x hub is connected downstream to this port, the USB 3.0 portion of the hub and the USB 2.0 portion of the hub could be reported on two different ports…
Part Number: TUSB320LAI Other Parts Discussed in Thread: TMUXHS4212 , TPS25821 , TUSB321AI , ESD441 Tool/software: Hi Team,
Customer wants to replace an USB OTG interface with USB-C DRP (USB3.2 up to 1.5A) and use the TUSB320LAI for this use case.
Can…