Part Number: TPS25831-Q1 Hi Team,
I have two questions.
-------
[Q1]
I would like to know the actual resistance value between CCx(CC1/2) and GND.
Could you please let us know if you have any information?
[Q2]
If the TPS25831-Q1 is turned off with the…
Part Number: TPS25831-Q1 Other Parts Discussed in Thread: TPS25830-Q1 , Hello Team,
Thanks for your support.
I understood the TPS25830-Q1 is for SDP/CDP, and TPS25831-Q1 is for DCP application.
Is there any difference about DCDC converter spec?
Regards…
Part Number: TPS25831-Q1 I'm using a TPS25831 in my design, but it is not behaving as expected. It isn't generating the 5V output when a device is attached to the USB-C connector. I've got it configured in DCP mode.
With no device attached…
Part Number: TPS25831-Q1 Hello support team,
We are considering using TPS25830 and TPS25831, so we have two questions about these ICs.
(1) Do these ICs support the MFi OCP spec?
You said they can support it in a previous thread, but we're wondering if…
Part Number: TPS25830A-Q1 Other Parts Discussed in Thread: TPS25831-Q1 Hi team,
Customers want to know how large the current is when TPS25830A-Q1 cannot support DCP AUTO.
In my understanding, when apple device connect the charger with a type-C connector…
Part Number: TPS25831-Q1 Other Parts Discussed in Thread: TUSB320 , TPS25830-Q1 , , TPS25840-Q1 We have a CPU with a USB2 OTG port. Now we are going to connect this port with a USB type C connector. The USB C acts as the host and device. In host mode, we need…
Part Number: TPS25831-Q1 Other Parts Discussed in Thread: TPS25831Q1EVM-062 We are using TPS25381 on our circuit:
• When 8 V < VIN ≤ 19 V, the switching frequency of TPS2583x-Q1 is determined by RT resistor or external sync clock.
We found…
Part Number: TPS25831-Q1 Hello,
What dithering scheme is used in TPS25831-Q1 such as triangular or pseudorandom?
What is the modulation frequency, which includes how wide it is spread, and how quick the frequency changes back and forth?
My customer would…
Part Number: TPS25830A-Q1 Tool/software: Hi team,
TPS25830A-Q1 CDP can charge by 5V/3A? Also TPS25831 DCP can charge by 5V/3A?
And both of charge method meet USB standard?
Regards,
Youhei MIYAOKA