Part Number: TPS25832-Q1 Other Parts Discussed in Thread: TPS25832A-Q1 Tool/software: Hello,
Q1-) I don't see much difference between the two part numbers below, which one do you recommend I use in my new design?
Q2-) What is the difference between…
Part Number: TPS25832-Q1 Other Parts Discussed in Thread: TUSB320
Hello,
Unfortunately, setting CTRL1 and CTRL2 lines to LOW is not working for client mode. We have now a design and tried this to download our software to the processor. But the processor…
Hello Hanno,
The TPS25833-Q1 does not have data switches on DP and DM. The alternate variant of this device is the TPS25832-Q1, which has data switches. Note that pins 7 and 8 of the TPS25833-Q1 are dedicated for thermal sensing.
Is Audio Adapter Accessory…
Part Number: TPS25832-Q1 Hello,
We want to use the TPS25832-Q1 most time for connecting USB-Sensors to a custom processor board. It is implemented as USB-C lite, because only USB 2.0 lines are connected.
So it is an USB 2.0 connection in an USB-Type C…
Part Number: TPS25832-Q1 Other Parts Discussed in Thread: TPS25833-Q1 Hello Team,
We had planed to use this for Car charger.
Annual volume required is 50K/year
SOP:2021
Customer: Nissan
We would like to know the schematic using this part with below…
Part Number: TPS25832-Q1 Other Parts Discussed in Thread: TPD6S300 , TPS25833-Q1 Hello,
I want to use the TPS25833 to have an USB-C connection on an USB 2.0 Hub.
My idea is to have a 5 port USB 2.0 Hub. 4 downstream ports are used with normal USB-Type…