Part Number: TPS25830A-Q1 Other Parts Discussed in Thread: TPS25833-Q1 , TPS25854-Q1 Hi team
What key feature diffrence between TPS25833-Q1 and TPS25854-Q1?
Thank you
Best regards
Part Number: TPD2E2U06-Q1 Other Parts Discussed in Thread: TPS25854-Q1 , , TPD4E02B04-Q1 , ESD321 Tool/software: Hi team,
Could you help select suitable ESD protection device selection for TPS25854-Q1 D+ and D-? Below are candidate.
2ch: TPD2E2U06…
Part Number: TPS25854-Q1 Other Parts Discussed in Thread: TPS25846-Q1 , , TPS25830A-Q1 , TPS25772-Q1 , TPS55289-Q1
Tool/software:
Dear TI experts,
My customer prepare the project of wired USB charging solution for car.
I suggested some parts based…
Part Number: TPS25854-Q1 Tool/software: Hi team,
External ESD protectoin is for TPS25854-Q1 D+ and D-, whose absmax are +6V, are considered.
On the ohter hand, ESD protection device breakdown voltage are higher than TPS25854-Q1 absmax.
As…
Part Number: TPS25854-Q1 Tool/software: Hi,
1. Is it okay to seal an IC with resin encapsulation by potting? I'm thinking of using urethane resin or epoxy resin as the potting material.
2. Please let me know if there are any conditions for resin sealing…
Part Number: TPS25854-Q1 Other Parts Discussed in Thread: LM74700-Q1 Tool/software: Dear team,
Will it be the problem on IC behavior if we place the reverse current block diodes at BUS out line? We like to place it to protect IC from unexpected OV or…
Part Number: TPS25854-Q1 Tool/software: I am currently working with the TPS25854-Q1 evaluation module and would like to request the original schematic and artwork files for the TPS25854Q1EVM . The images in the datasheet are not sufficient, as I need…
Part Number: TPS25830A-Q1 Other Parts Discussed in Thread: TPS25854-Q1 , Hi team
I see in TPS25830A-Q1 DS there is no DCP Auto Mode description like TPS25854-Q1, but it can support multiple USB charge protocol, which can be seen in DS 10.3.15 USB Specification…
Part Number: TPS25854-Q1 Tool/software: Hello TI team,
We are currently developing a 65W GaN fast charger featuring two USB Type-C ports and one USB Type-A port . The design includes two InnoSwitch INN3368C chips operating in parallel on the input side…
Part Number: TPS25854-Q1 Hello, My customer is not familiar with USB charger spec and has a couple of questions about TPS25854-Q1 current limit as follows. Q1: Datasheet 10.3.8.1 says “For the normal application, it can short the ILIM pin to GND directly…